Part Number: TCAN1145EVM
Hi,
I have a TCAN1145EVM board at hand with selective wakeup function configurated, but it can not be waked up by the CAN frame even if I set the ID mask to all "1". Can you tell what the reason could be?
The TCAN1145 ID filter is set as 0x102, ID mask is set as 0x7FF, the baud rate is set as 500KHZ. the SWCFG and SW_EN flag are set in the last two step. All these registers value are read back from TCAN1145 and saved in "TCAN1145_Wakeup_CFG" as the screenshot shown below. But no matter what CAN signal (0x102, 500KHZ)is sent to TCAN1145, it always stays in sleep mode rather than enters standby mode. What could be the reason?

Thank you,
Hao