Part Number: TPS65987D
Hello team,
I have received a replacement question from my customer about the USB PD controller TPS65987D.
My customer is searching for a PD controller which could be a replacement of the TPS65987D because of supply issue.
Could you recommend us if there are proper device that meets system requirements listed below?
- USB Type-C 1port
- USB 3.1 Gen2 (10Gbps)
- DisplayPort 1.4(Alternate mode)
- USB PD 3.0(DRP or Sink, 15V 45W)
As far as I searched, I couldn't find a device that could fulfill both USB3.2 and DP1.4. I would like to confirm just in case.
Best Regards,
Ryotaro Fukui