Part Number: TUSB8043A
I have tested USB3.2 undernal the following conditions,
But no test signal is output.
1:The DTU is turned on, If the DTU is peripheral, Vbus is supplied from the USB connector.
2:There is a tceduermination (50OHM) on the Tx line of DTU.
3:The connection partner does not respond to the LFPS signal transmitted by DTU and times out.
Is this procedure correct?
Thanks
Hiroyuki Takada