Part Number: TPD12S521
Hi,
My customer has the following questions. Could you please answer them?
*1.
According to the following figure.2 on the datasheet P.1, DCLK_OUT signal is pull-up on 5V. Also, on Sink side, 47kohm pull-up is required on DCLK_OUT.

On the case that Source side (TPD12S521) is power-off and Sink side (outside of HDMI connector) is power-on, is it possible that leak current is occurred from outside equipment (47kohm pull-up) to TPD12S521 equipment?
*2.
If yes, could you please propose how to protect this leak current?
*3.
According to IBACK DRIVE parameter on datasheet P.5, MAX current is 5uA. Is this included CEC pin? On HDMI specification, when source is OFF, CEC leak current is less than 1.8uA. Can TPD12S521 meet this specification? Please advise us.
Thanks and best regards,
M.HATTORI