Part Number: MAX3232E
HI,
Could you provide information on the current consumption of the transceiver IC under the following conditions?
Devices : MAX3232EIPWR and MAX3232IPWR (probably the same current consumption)
ON Channel : 2TX / 2RX
Capacitive load : 100pF
Resistive load : Connect two TX-RXs of the same device.
I think that only the built-in pull-down 5k is available in this case. Correct?
Data rate : 36800bps / 250kbps
Looking at another thread, I found out that TI engineers can provide similar information.
I would be grateful if you could give me an answer.
Best regards,
Hiroshi