Part Number: DS90UB941AS-Q1
Dear TI:
Or it has nothing to do with UB941/UB948? Our design is soc -> UB941 -> UB948, Please help, thanks.
BR,
Arvin
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: DS90UB941AS-Q1
Dear TI:
Or it has nothing to do with UB941/UB948? Our design is soc -> UB941 -> UB948, Please help, thanks.
BR,
Arvin
Hello,
The UB948 can be configured to output RGB888 or RGB666 with either JEIDA or VESA mapping schemes. Mapping scheme selection is controlled by the MODE_SEL0 pin or may be overridden in register 0x49.
Regards,
Ben Dattilo
Hi Ben:
Which one is ok? Configured to 0x61/0x41/0x60/0x40? Thanks.
Br,
Arvin
Hi Arvin,
If you want 24-bit Dual FPD-Link JEIDA format (LSB on D3/D7) as shown below, writing 0x40 to register 0x49 will do this.
Regards,
Ben