This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN65LVDS822: similar replacement option

Genius 17445 points

Part Number: SN65LVDS822
Other Parts Discussed in Thread: DS90CR286AT-Q1, DS90CR286A-Q1, SN65LVDS86A-Q1

Hi all

My customer has a design with the SN65LVDS822.

Because of the constrained market they are looking for a potential replacement option.

Is there a similar device the customer could look at ?

Best regards

Ueli

  • Hello Ueli,

    Can you share some of the features and device specifications that your customer is looking for? What is their application?

    Can I get some background that will be help me find and decide the most relevant replacement choice for you?

    Thank you,

    Best Regards,

    Shruti More

  • Hello Shruti

    Thank you for the quick reply.

    Please find the customer feedback below.

    Best regards

    Ueli

    ---------------------

    We control an LCD display 480x800 Pixel with a parallel RGB interface (18Bit, 6-red 6-green 6-blue). From the CPU-Board the display control signal are LVDS. With the TI SN65LVDS822 LVDS deserializer we get back the parallel RGB signals. The display clock (pixel clock) frequency is around 30MHz.

     

  • Hello Ueli,

    Based on the information you provided, we suggest you consider the following devices for replacement:

    1. DS90CR286AT-Q1 --- 3.3 V Rising Edge Data Strobe LVDS Receiver 28-Bit Chan Link 66 MHz

    2. DS90CR286A-Q1 --- +3.3V Rising Edge Data Strobe LVDS 28-Bit Automotive Channel Link Receiver - 66 MHz

    3. SN65LVDS86A-Q1 --- Automotive catalog FlatLink receiver (maybe you'd prefer number 1 and 2 more).

    I believe all these devices are available to buy from distributors, if they are not in stock on ti.com. 

    Hope this helps.

    Best Regards,

    Shruti More

  • Hello Shruti

    Thank you for these recommendations.

    Best regards

    Ueli