Part Number: DS90UB954-Q1
Hey,
I use the serializer/deserializer combination DS90UB954/53 with the MIPI-CSI sensor OS08A20 on Jetson NANO.
I got this strange ghosting of older frames transparently overlapping new frames when used with serializer/deserializer. Without changing any configuration when I use the camera directly on CSI port this ghosting is not visible, so I guess it somehow has to come from the serializer/deserializer. Do you guys have any idea what register settings could cause this kind of behaviour? You can see the effect in this video I posted in the NVIDIA Jetson forum. Please have a look! https://forums.developer.nvidia.com/t/nvarguscamerasrc-ghosting-from-previous-frames/184759
0 1 2 3 4 5 6 7 8 9 a b c d e f
00: 60 00 1e 20 df 01 00 fe 1c 10 7a 7a bd b9 00 00
10: 00 00 c1 00 00 00 00 00 00 00 00 00 00 00 04 02
20: 20 01 00 00 00 00 00 00 00 00 00 00 00 00 00 00
30: 00 00 00 41 40 01 00 01 00 00 00 01 14 6f 00 40
50: 00 00 00 03 00 00 00 00 de 00 00 30 30 00 00 00
60: 00 00 00 00 00 00 00 00 00 00 00 00 00 7c 99 99
70: 2b 2c e4 04 38 09 60 c5 00 01 00 00 20 00 00 00
80: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
90: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
a0: 02 0f 00 00 08 19 00 00 00 00 00 00 00 00 00 00
b0: 08 14 3f 00 25 00 18 00 8c 33 83 74 80 00 00 00
c0: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
d0: 00 43 94 04 60 f2 00 00 00 00 00 00 00 00 00 00
e0: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
f0: 5f 55 42 39 35 34 00 00 00 00 00 00 00 00 00 00
i2c-dump UB953
0 1 2 3 4 5 6 7 8 9 a b c d e f
00: 30 00 33 48 00 03 41 28 fe 1e 10 7f 7f f0 f0 00
10: 00 00 00 00 00 20 18 3c 80 62 62 62 00 00 00 00
20: 00 00 00 00 00 02 00 00 67 33 01 00 00 00 00 00
30: 00 20 88 04 00 10 00 60 00 00 00 00 00 00 00 00
40: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
50: 20 c0 45 00 00 00 00 00 07 07 07 00 00 00 00 00
60: 00 2b 60 09 1d 88 00 00 00 00 00 00 00 00 00 00
70: 00 00 25 00 00 00 00 00 00 00 e4 00 00 00 00 00
80: 00 00 00 00 00 00 90 00 00 00 00 00 07 00 00 00
90: 32 e3 64 01 00 00 00 00 00 00 24 22 00 0a 06 12
a0: 00 10 12 0f 0e 10 42 10 10 10 03 01 00 00 00 00
b0: 04 4a 3f 00 00 00 00 00 00 00 00 00 00 00 00 00
c0: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
d0: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
e0: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
f0: 5f 55 42 39 35 33 00 00 00 00 00 00 00 00 00 00