Part Number: SN75240
Other Parts Discussed in Thread: SN65220, , SN65240
Hi support team.
I have received the following inquiries from my customers who are already using this device in mass production.
1. In DESCRIPTION (page1), it changed as follows.
I would like to know when and why the change was made.
Rev.F
The SN65220 is a single transient voltage suppressor and
the SN65240 and SN75240 are dual transient voltage
suppressors designed to provide electrical noise transient
protection to Universal Serial Bus (USB) 1.1 ports.
Rev.I
The SN65220 device is a dual, and the SN65240
and SN75240 devices are quadruple, unidirectional
transient voltage suppressors (TVS). These devices
provide electrical noise transient protection to
Universal Serial Bus (USB) low and full-speed ports.
2. In ABSOLUTE MAXIMUM RATING
Rev.F has a description of Continuous power dissipation,
It is no longer Rev.I.
Could you tell me the reason for this?
Thank you for your cooperation.
Best regards
Higa