Part Number: TUSB8020B
Hi,
My customer has the following several questions. Could you please support us?
*1. When all register values are used with default values, are 2pin:SCL/SMBCLK, 3pin:SDA/SMBDAT, 22pin:SMBUSz/SS_DN2 "open"?
*2, After 8.5.1.11 Device Configuration Register 2 (offset = Ah), there is no Reset value on each Table. Is the value listed in Figure xx. Resister Offset xh a Reset value?
*3. Register values listed in "Figure xx. Resister Offset xh" shows "X" What does the X mean? For example, 1:0 bit in Figure 10. Register Offset 7h is X.
*4. What does the X in 0Xh mean as the reset value in Table11? Other Tables may have similar notation.
*5. On "8.5.1.6 Device Configuration Register (offset = 5h) [reset = 1Xh]", bit_5 enables/disables U1/U2. What does U1/U2 mean?
*6. On "8.5.1.8 Device Removable Configuration Register (offset = 7h) [reset = 0Xh]", What determines whether a device can or cannot be removed?
Thanks and best regards,
M.HATTORI.