We are developing a new product which uses DS90UB947&DS90UB948 for display function. About 947&948, I have a question as follows:
The SOC we are using has two LVDS independent channels, and for 1080P@60fps display requirement, we use these two LVDS channels to transfer the video data to the display device via FPD-LINK III.
But we found something different between 947&948, is that there is only one pixclock input channel of 947, and the SOC and 948 all have two channels( odd and even channel). So why 947 has only one PCLK
channel? And which PCLK should we choose to input from SOC to DS90UB947? Thanks!