This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TUSB1002EVM: Continuous transmission link more than 5m distance

Genius 9880 points

Part Number: TUSB1002EVM
Other Parts Discussed in Thread: TUSB1002A, TUSB1002, TUSB216I

Hi,

Customer is having a continuous transmission problem in a more than 5m distance.

Customer aims is to transmit USB 3.2 Gen1 over the whole transmission path. Their biggest problem is the 10m cable between two ODU connectors. According to them, this should be continuous. On the red marked positions we can place some electronic which can help to amplify the transmitted signal.


They tried to build up a transmission link with the TUSB1002EVM. Until now they succeed no continuous transmission link with more than 5m which can transmit USB 3.2 Gen1.
 

Is there any alternative solutions, any alternative products which can provide the appropriate gain and compensate the cable loss?

Regards,
Maynard