Hi Team,
A customer is looking into the TPS65988 and is wondering if there is an integrated feature within the TPS65988 that will allow for the device to be used in a USB-C PD application leveraging authentication. What I mean by this - is there a way to verify that the TPS65988 only delivers power/allows data to be transferred to specific devices even if a device properly attaches to the USB-C port? I did not see anything in the datasheet, so I wanted to make sure I didn't miss anything. If there is not an integrated feature I'm also curious if its possible to implement using logic.
Thanks in advance,
Vijay