This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TUSB4020BI: Input Current

Expert 5296 points

Part Number: TUSB4020BI

Hello, 

I am planning on using 1 TUSB4020 and 1 TUSB4041. They will be both powered off 1.1V supply and we would like to use a single Vreg to power both. 

Can you please confirm the input current and Icc requirement? 

Would a 500mA regulator be enough to power both a TUSB4020 and TUSB4041? Are the below current values form the datasheet absolute maximums? 

From TUSB4020BI datasheet section 7.6, the input supply current is shown below:

 

From the TUSB4041 datasheet section 7.7:

Thanks!