Part Number: TLK100
Hi.
I'm going to use TLK100 with 3.3V power only.
How much current can V18_PFBOUT(pin number 40) output ?
I want to connect logic ic power(LV14 or LV2G) only. Is this no problem ?
Best regards.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TLK100
Hi.
I'm going to use TLK100 with 3.3V power only.
How much current can V18_PFBOUT(pin number 40) output ?
I want to connect logic ic power(LV14 or LV2G) only. Is this no problem ?
Best regards.
Hello,
Thank you for the query. The core voltage is specified as 1.55. You should be able to use few micros of current but would need to be tested with the device on the behavior during powerup or reset.
Where did you get the 1.8V number ?
Also please check the pin number
https://www.ti.com/lit/ds/symlink/tlk110.pdf
Regards,
Sreenivasa
Hi.
Thank you for reply.
I use TLK100.
https://www.ti.com/product/TLK100
TLK100 evaluation board use V18_PFBOUT(pin number 40) for osc.
Best regards.
Hi.
I add one question.
Please tell me the voltage accuracy of V18_PFBOUT(pin number 40).
Best regards.
Hello
The supply rang is 1.7 to 1.9V. The PFBOUT is expected to be within this range.
Regards,
Sreenivasa
Hi.
Thank you for quick reply.
How much current can V18_PFBOUT(pin number 40) output ?
Best regards.
Hello,
The PFBOUT is an infernal regulator optimized to generate the supply rails for the device operation.
They are not expected to power any external loads. Since you wee looking to power a simple gate, this seemed acceptable.
I do not see the LDO current specification mentioned that i could share or point to.
Regards,
Sreenivasa