Part Number: SN65DPHY440SS
Hi Team,
We have used SN65DPHY440SS Retimer in our Camera project. We have two different Image sensors ( OV8856 & OS08A20 ). Both are 8MP sensors. Our data rate is 800Mbps. We are observing some data error when using OS08A20 sensor with the Retimer. Image is not getting. Below are our observation.
1. OV8856 with Retimer
This is working. Image is getting properly. This is the eye diagram below.

2. OS08A2 with Retimer
This is not working. Obtained image is blank. This is the eye diagram below.

3. OV8856 without Retimer
We made this test setup by removing Retimer IC and shorted the trace with jumper wires. This is also working fine. Image is getting properly. This is the eye diagram below.

4. OS08A2 without Retimer
Same test setup as OV8856 without Retimer and trace are shorted. This time we obtained proper image. This is the eye diagram below.

We are wondering why OS08A2 is not working with Retimer and at the same time OV8856 is working. Similarly OS08A2 is working perfectly without Retimer using traces shorted. The retimer was in default hardware configuration initially. After that we tried different options by changing Equalization, Egde rate control and TX emphasis, but still it didn't work for OS08A2, at the same time it was working with OV8856 except for Equalization at 5dB. We are not giving any configuration via I2C. Schematics below.

Please let us know if we need to do anything to configure the Retimer for this application.