Other Parts Discussed in Thread: ALP
Hi,
I am studying 92x products recently, and I want to transfer I2S signal through FPD-Link.
I use 924EVM and 927EVM pair to transmit i2s signal through FPD-link, but I can't get the SCLK signal from 924 side.
I have successfully received WC and data signal in 924 side except SCLK, though I use the same configuration for the related pins.
I have checked the sclk waveform in 927 side which is OK, but no waveform shows in CLK pin in 924.
WC and DATA signals show in both side are the same and correct.
Could please help solve such problems?
Thanks.
The following is my configuration for 924
Register Display - ALP Nano 1 - DS90UB924, Connector 1
Register Data Name
0x0000 0x58 I2C Device ID
0x0001 0x04 Reset
0x0002 0x00 General Configuration 0
0x0003 0xF0 General Configuration 1
0x0004 0xFE BCC Watchdog Control
0x0005 0x1E I2C Control 1
0x0006 0x00 I2C Control 2
0x0007 0x36 Remote ID
0x0008 0x00 SlaveID[0]
0x0009 0x00 SlaveID[1]
0x000A 0x00 SlaveID[2]
0x000B 0x00 SlaveID[3]
0x000C 0x00 SlaveID[4]
0x000D 0x00 SlaveID[5]
0x000E 0x00 SlaveID[6]
0x000F 0x00 SlaveID[7]
0x0010 0x00 SlaveAlias[0]
0x0011 0x00 SlaveAlias[1]
0x0012 0x00 SlaveAlias[2]
0x0013 0x00 SlaveAlias[3]
0x0014 0x00 SlaveAlias[4]
0x0015 0x00 SlaveAlias[5]
0x0016 0x00 SlaveAlias[6]
0x0017 0x00 SlaveAlias[7]
0x0018 0x00 Mailbox[0]
0x0019 0x01 Mailbox[1]
0x001B 0xF4 Frequency Counter
0x001C 0x03 General Status
0x001D 0x25 GPIO0 Config
0x001E 0x55 GPIO1 and GPIO2 Configuration
0x001F 0x00 GPIO3 Configuration
0x0020 0x00 GPIO_REG5 and GPIO_REG6 Configuration
0x0021 0x22 GPIO_REG7 and GPIO_REG8 Configuration
0x0022 0x52 Data Path Control
0x0023 0x10 Rx Mode Status
0x0024 0x08 BIST Control
0x0025 0x00 BIST Error
0x0026 0x83 SCL High Time
0x0027 0x84 SCL Low Time
0x0028 0x00 Data Path Control 2
0x0029 0x00 FRC Control
0x002A 0x00 White Balance Control
0x002B 0x04 I2S Control
0x0035 0x00 AEQ Control
0x0039 0x00 PG Internal Clock Enable
0x003A 0x00 I2S DIVSEL
0x003B 0x03 Adaptive EQ status
0x0041 0x03 Link Error Count
0x0044 0x60 Adaptive Equalizer Bypass
0x0045 0x88 Adaptive EQ MIN/MAX
0x0049 0x00 Map Select
0x004B 0x08 LVDS Setting
0x0056 0x08 Loop-Through Driver
0x0064 0x10 Pattern Generator Control
0x0065 0x00 Pattern Generator Configuration
0x0066 0x00 PGIA
0x0067 0x00 PGID
0x006E 0x00 GPI Pin Status 1
0x006F 0x00 GPI Pin Status 2
0x00F0 0x5F RX ID
0x00F1 0x55 RX ID
0x00F2 0x42 RX ID
0x00F3 0x39 RX ID
0x00F4 0x32 RX ID
0x00F5 0x38 RX ID
Regards,
Cathy