Part Number: TLK10031
Hi,
My customer is interesting to TLK10031. The datasheet says this device support 10GBASE-KX. My customer want to know if it support 10GBASE-ER application?
Thank you!
John
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
Yes, the TLK10031 supports 10G SFI interfaces to all SFP+ limiting variants including ER. The host simply needs to use KR settings except disable both auto-negotiation and link training.
Thanks,
Rodrigo Natal
Thank you for reply.
The datasheet says operation mode can be selected through pin (MODE_SEL/ST) or register 1E.0001 bit10, while I cannot find detailed description about Reg 1E.0001. And also datasheet does not explain how to select operation mode through MODE_SEL and ST pin.
Could you please let me know how should I configure the part to operate in SFP+ mode through pin and regester?
Regards,
John
Hi,
The datasheet does capture the details you are requesting.


The TLK are registers are set up for KR mode by default. For SFP+ interface cases the user should disable AN and link training via MDIO registers. See below.


Thanks,
Rodrigo Natal