This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS65988DJ: Ask for support doesn’t use TBT3 or follow Intel reference design

Part Number: TPS65988DJ


We have an application that doesn’t use TBT3 or follow Intel reference design. Unfortunately we designed and manufactured it with TPS65988DJ (which TI suggests to use with TBT3 ref design only) instead of TPS65988DH (for general use). Changing to TPS65988DH isn’t an option for us right now.
Our application only needs to detect capability of device connected to USB C port (source, sink wattage, DFP, UFP).
Can you help to confirm if those features are still able with TPS65988DJ? If yes then how can we archive it (use configuration tool to config then have the patch sent to PD or what else do we need to do?)
The TPS6598x configuration tool on TI website doesn’t support DJ. We logged a request to get the tool. Can you support us on that?