Part Number: MAX3243E
Hi Team,
Does MAX3243E support RS422/RS485 interface?
If no, do we have solution can support them?
Best regards,
Hardy
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Hardy,
This device is an RS-232 transceiver, which is quite different than an RS-485 device. Namely, RS485 (expanded from RS-422) is a differential signaling protocol. You may want to check out our RS-485 portfolio here.
Let me know if you have any more questions.
Regards,
Eric Schott
Hi Eric,
My customer is seeking P2P solution with MAXLINEAR SP339E. But I have checked ti.com and don't find P2P solution.
Could you suggest TI same function with competitor part?
The SP339E datasheet as below link.
https://www.maxlinear.com/ds/sp339e.pdf
Best regards,
Hardy
Hi Hardy,
This part is a specialized device that contains both RS-232 (3TX/5RX) and RS-485 (half or full duplex) transceivers. We don't offer any such device that integrates both types of transceivers into the same package. However, I can recommend solutions for each use independently.
For the multichannel 1Mbps RS-232 line driver/receiver, I can recommend the SN75C3243.
For the RS-485 transceiver, it will depend on if you are currently using half-duplex or full-duplex mode. For this, I can recommend THVD1450 or THVD1452 for half-duplex or full-duplex respectfully. Note that these transceivers do not have integrated termination so a resistor will need to be placed externally if required for that node.
Regards,
Eric Schott