Part Number: SN65DSI83
Hi Team,
For InnoLux G156BGE-L03 15-inch LCD panel,
Try to adjust the combination of LVDS timing, but it has been unstable,
The current situation is that if the machine is turned on and off for 10 times, the LCD screen or color will be abnormal 3~4 times on average.
The following is the adjusted timing, can you help review and provide the following 6 sets of better suggested values for timing.
Hsync front porch = 82, Hsync back porch = 52, Hsync pulse width = 60
Vsync front porch = 14, Vsync back porch = 12, Hsync pulse width = 12
The above 6 sets of timing are set based on the following frequency conditions.
Clock Frequency = 76MHz, H_Active = 1366, V_Active = 768
Hsync polarity = Vsync polarity = positive polarity
The display timing specification of InnoLux G156BGE-L03 is as follows