Part Number: TUSB8020B-Q1
Hi,
Would like to confirm on few matters:
1. On pin4 (BATEN1) and pin 6 (BATEN2), do they output high when there is VBUS input to the voltage divider at pin 9?
2. If downstream port 1 does not require VBUS and downstream port 2 requires VBUS to power up USB device (but not battery charging), do the pin4 and pin 6 still require the 4.7kOhm pull up to 3.3V?
3. For above configuration, can i leave pin 36 (FULLPWRMGMTz) open as the upstream port is SS USB capable port?
Thanks.