This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS90UB913A-Q1: Maximum value of tJINR

Part Number: DS90UB913A-Q1

Hi team,

Could you advise the maximum value or distribution of tJINR in order to calculate the jitter budget?

tJINR is specified as 0.016UI typ.

regards,

  • Hello Shinji,

    We do not spec max value or distribution of this parameter. There is no need to use this parameter as part of your system design - for 913A please focus on the serializer input jitter and for the FPD channel please focus on the channel s-parameter requirements to ensure operation 

    Best Regards,

    Casey