Part Number: TPS25750
- in Figure 9-22 of P.40 of TPS25750 datasheet, we would like to use TPS25750 ADC to read the VBUS voltage(5V~20V)/ current(500mA~3A). Do we need add external voltage divider2 and I-to-V circuit? And how to control the input mux and read ADC value
- our product is a power bank(sink only), which can support upto 20V/3A adaptor input. We see there are 3 Dea Battery Configuration(AlwaysEnable Sink, NegotiateHighVoltage, SafeMode), configured by ADCIN1/ADCIN2.
# AlwaysEnableSink -
- does it mean source detect TPS25750 Rd, and output 5V?
#NegotiateHighVoltage -
- it meantions that "this cannot be used when a patch is loaded from EEPROM", what's the reason?
- what does patch mean? initial registers?
#SafeMode -
- it meantions that "the device does not enable the sink path". But how does system get powered in dead battery mode w/o sink path?
- for our product(power bank sink only), do u recommend to use AlwaysEnableSink mode, we use 5V to bootup the system, then control TPS25750 to negotiate to 20V, is it correct?
- we found I2C Vih is 1.3V/ Vil is 0.54V in P20 of TPS25750 datasheet, does it mean we can use I2Cs is 1.8V I2C? Our MCU is 1.8V I2C