Part Number: DP83TC811S-Q1
In Chinese:
Hello,
我们使用网卡型号是DP83TC811S-Q1,请问是否支持PHY层外部回环,如果支持如何打开?
非常感谢!
In English:
Hello,
We want to know if this ethernet card support the outer loop(back), if support, how we should open it?
Thank you very much!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: DP83TC811S-Q1
In Chinese:
Hello,
我们使用网卡型号是DP83TC811S-Q1,请问是否支持PHY层外部回环,如果支持如何打开?
非常感谢!
In English:
Hello,
We want to know if this ethernet card support the outer loop(back), if support, how we should open it?
Thank you very much!
Hello Zhang Lorry
Thank you for the query.
Can you help us understand which ethernet card you are referring to.
If you are referring to reverse loopback, please see below
Regards,
Sreenivasa
Hello Zhang Lorry
Thank you for the inputs.
Yes, loopback modes are available in the device and allowed.
Regards,
Sreenivasa
if I want to close/ open the external loopback modes, what I should do, eg. change the properties in the which config file or execute some command.
Or we can't close the mode.
Hello Zhang Lorry
Thank you for the message.
Is this question related to the driver. Which MAC are you using ?
Regards,
Sreenivasa
Hello, Kallikuppa
Thanks for you reply.
we can't get the mac model easily, currently we use qcom sa6155 borad(we can't easily get the MAC model in office document), can you tell me how I can get the MAC model you request?
Thank you very much
Hello Zhang Lorry
Thanks. I see that you are using the qcom sa6155 board. Have you reached out to qcom for help.
I will check internally if and see how best i can help. I expect to comeback by early next week.
Regards,
Sreenivasa
Thanks Kallikuppa!
Before you check, I want to konw, different MAC, the way open/close the external loopback is different?
Or do you mean some version MAC don't support loopback?
Thank you very much
Hello Zhang Lorry
Thanks. The question i has was not different mac but which MAC you are using. You mentioned this is qcom sa6155 board and i got the answer.
I assume you are using the drivers from qcom..
Regards,
Sreenivasa
Hello, Kallikuppa
In fact I just want to konw there is anyway(change config or or invoke some api) we can close/ open loopback; for we will do test the ethernet output through, bit erro rate and so on;
so we must make sure the ethernet card is "supported external loopback" and "the external loopback function is open".
Thank you very much!
Hello Hello Zhang Lorry
Thank you for checking. Have you reached out to qcom.
I will let you know if i have some inputs.
Regards,
Sreenivasa
Hello Zhang,
I am closing this thread as I understand that this has to be resolved with help from MAC side. From PHY side, let me know if you need help to enable any specific loopback mode mentioned in datasheet.
--
Regards,
Vikram