Part Number: TPS25750
Hi sir,
I have a query on source detection and charging settings of TPS25750.
If I wanna change of source detection and charging settings,
Can I create custom applications through GUI tools?
When the charging current is controlled according to the detected specification on the source side
How to set it on the GUI tool?
Or will the IC automatically limit and adjust the current?
Set the charging voltage and charging current in settings 9 ~ 12 on the GUI tool.
Is this the value when the condition for requesting sink power selected in setting 3(15W/5V) is met?
If the detected power supply specification on the source side does not meet the conditions selected in setting 3 (15W/5V),
or What kind of control will be carried out when the charging cannot be carried out under the set charging conditions?
For example, for the setting of 15W (5V / 3A), when 7.5W (5V / 1.5A) of USB type-C is connected
Imagine using a USB a to C cable to connect to a charger or USB port other than type-c.
What happens?
Thanks for your clarification.
Regards,