Part Number: TUSB546A-DCI
Other Parts Discussed in Thread: TUSB544, TUSB564, TUSB1064, TUSB422
Team,
Can you please help with the below follow up questions.
USB3 is not require. Here are 3 possible options are:
TUSB544 –> TUSB544
TUSB546A –> TUSB564
TUSB1046A –> TUSB1064
a)Is TUSB546A required even if USB3 is not used?
Are there additional options apart of the one above?
b)Which cable lengths can I compensate with the components mentioned above (depending on the cable cross-section)?
c)What additional components do I need to be able to use Alt Mode (signal rotation depending on connector orientation, PD controller... )?
Presumably we need the TUSB422 plus an MCU as controller. Anything else needed?
d)Do the USB controllers run stand-alone? Are these fully programmed and ready to run immediately?
e)What are the advantages of the TUSB546A/TUSB564 devices over the TUSB544?
Obviously, the TUSB544 does not have a mux for flipping the polarity, does it? How does the flip feature work then?
Thanks in advance!
A.