This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS65987D: SPI_PICO/SPI_POCI

Part Number: TPS65987D

Hi Team,

there are the different pins 37/38 names on the different pages of the TPS65987D datasheet.

Where is correct?

Also what's right for the boot mode: Table 8-5. Boot Mode Pin Strapping ? MOSI or MISO should be tied to 1/0?

Document revision:SLVSES1C – MAY 2018 – REVISED AUGUST 2021

  

  • Hi Eugene,

    It looks like the first image is incorrect. This will be corrected and updated in the next revision. Please use the pin descriptions section from your second image for the correct pins.

    For the boot pin strapping, it is the SPI_POCI which is labeled correctly, it was previously the MISO pin.

    Thank you,

    Hari