Part Number: TUSB1002A
Hi,
I have a system that failed receiver jitter tolerance test for USB3.2 gen 2.
It managed to pass Tx compliance tests for USB3.2 gen 2. No issue with USB3.2 gen 1 for Tx compliance and Rx jitter tolerance tests.
The estimated channel losses are shown in figure below. The Tx and Rx EQ were set to 9.0dB and 5.5dB respectively.

Any idea on how to improve the receiver jitter tolerance? I don't have the equipment for USB3 testing and rely on third party lab to help out on the compliance test. Hence, trial and error method is not easy for me.
Thanks.
Regards,
Yi Fan