Part Number: TCAN4550-Q1
Other Parts Discussed in Thread: TCAN4550
Hello,
I am looking for operating characteristics curves for the TCAN4550-Q1 automotive chips, most notably efficiency curves of the component. It would seem that the device's datasheet is sparse on this type of data. Would it be possible to request them here ?
Additionally, I would like to take the opportunity to signal a very small issue with the section numbering of both TCAN4550's and TCAN4550-Q1's datasheets. It would seem that all register maps after Tx Buffer Add Request (Section 8.6.4.43) are incorrectly indented. The register map of Tx Buffer Cancellation Request should be Section 8.6.4.44, but it is labelled as Section 8.6.4.43.1 (sub-section to the previous register). This messes with the bookmarks of the PDF and makes just a bit harder to find info on certain registers from the document outline.
Best regards