This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS80PCI402: Min/Max spec for VTX-DIFF-PP (VOD) on 1.4Vpp setting

Guru 19685 points

Part Number: DS80PCI402

DS80PCI402 datasheet page-8 is described VTX-DIFF-PP (VOD): 0.8V_min to 1.2V_max

I guess that above VOD: 1.0V setting, and variation is ±20%.

Is it correct?

Please let me know about VOD variation in the case of VOD: 1.4V setting.

【Background】

One DS80PCI402 board tested on VOD: 1.4V condition, result was 0.8Vpp. 

I want to judge 0.8Vpp device is defect or acceptable operating range by any other points. 

By the way: 1.4V ±20% = 1.12V~1.68V.

Best regards,

Satoshi

  • Hi Satochi-San,

    VOD can vary between 0.8V to 1.2V. As long as the VOD is within this range, this should be acceptable.

    Regards ,, Nasser

  • Hi Nasser

    Thank you for reply,

    When VOD set 1.4V, this setting have no guarantee the VTX-DIFF-PP swing, correct?

    And, the other DS80PCI402 board tested on VOD: 1.4V condition, result was 1.22Vpp for out of the 0.8Vpp ~ 1.2Vpp range.

    Is this board possibility to defect?

    Best regards,

    Satoshi

  • Hi Satoshi,

    It is difficult to say this is a board defect. When measuring 1.22V versus expected 1.2V this may depends on the measurement setup, how VOD is measured, device setup, and scope bandwidth. 

    Regards ,, Nasser

  • Hi Nasser

    Thank you for reply,

    I summarized DS80PCI402 condition and question, please see below;

    【Condition】

    ・This application required VOD (= VTX-DIFF-PP): 1.4V setting

    ・One board measured VOD: 0.8Vpp, the other board measured VOD: 1.22Vpp (Out A+ to Out A-)

          

    ・Datasheet VOD swing range is 0.8Vpp to 1.2Vpp. (I guess VOD: 1.0V setting)

    ・When replace these two board and IC's (A-B-A test), VOD function is depend on implemented IC's. 

    【Question】

    ・Please let me know datasheet recommend VOD swing range the condition of VOD: 1.4V setting.

    ・Additional question, is there any setting for adjust the variation of VOD swing? 

    Best regards,

    Satoshi

  • Hi Satochi,

    1). Device has been characterized - across many parts - to have a range of 0.8V to 1.2V. Therefor we cannot specify 1.4V VOD.

    2). Please note table 8-3 of the DS80PCI402 data sheet. Level 13 can provide highest setting.

    Regards ,, Nasser

  • Hi Nasser

    Thank you for information,

    I understood specify of VOD: 1.4V.

    By the way, Table 8-3 written VOD: 0.8V to 1.3V setting, not include 1.4V.

    Is VOD: 1.4V setting unusual case on these IC or application?

    Best regards,

    Satoshi

  • Hi Satoshi,

    I had checked other parts as well and was not able to find a device with 1.4V swing. Typical applications require 300 to 750mV swing but i am not sure why your customer is needing 1.4V VOD. Based on my search, we do not have a part with guranteed 1.4V swing.

    Regards ,, Nasser