Part Number: TPS65988EVM
Other Parts Discussed in Thread: TPS65988
I have two TPS65988 boards connected with each other on a USB type C connecter. Both the devices are configured for alternate mode. Device A will send the VDM upon entering the alternate mode and Device B will receive it. My aim is to get that received VDM. I am referring SLVAE16A document for this POC. Device A will sink the power from Device B. I am using the EVK as a device B and my custom board as a Device A. I am using debug mode to check the received VDM. I checked register 0x61 for VDM but was not able to receive the VDM. I attached the configuration file for both the devices along with the screenshot of EVK. Please let me know why am not able to get the VDM on EVK? As you can see below the image I am not able to receive the sent VDO.