Part Number: TPS25750
Other Parts Discussed in Thread: BQ25792, , DRV8935
We have TPS25750D + BQ25792 so that BQ is attached to TPS I2Cm and MCU is in I2Cs.
Problem: If patch is loaded to TPS, charging is not working! Without patch, charging works.
I have generated following patch to TPS
{"questionnaire":{"version":"7.0.2.1","answers":[4,null,2,1,2,1,1,null,1,null,0,8,1.25,0.12,0.12],"options":{},"configID":"0000","vendorID":"0000"}}
Is some additional configuration needed?
Here is capture of TPS registers, after boot & charger attached: