This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DP83TD510E-EVM: DP83TD510 EVM bootstrap resistors

Part Number: DP83TD510E-EVM


Hello,

I have two DP83TD510 EVM,

I have a question regarding the configuration straps at jumper J20 and J18,

bootstrap low voltage < 0.6V
bootstrap high voltage > 1.3V

with J20 I can set pullup or pulldown either R26 or R201, but there is an additional Pulldown R92 installed.
with J18 I can set pullup or pulldown either R28 or R203, but there is an additional Pulldown R200 and Pullup R199 installed.

is it correct that R92,R200 an R199 are populated on the boards ?

Thanks

T.Fischer