Part Number: DS90UB962-Q1
Dear TI engineer,
According to the UB962 datasheet,it shows UB962 compatible to 4xUB935.
We want to know that do UB962 also compatible to 4xUB953 ?

Best regards,
Andy
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: DS90UB962-Q1
Dear TI engineer,
According to the UB962 datasheet,it shows UB962 compatible to 4xUB935.
We want to know that do UB962 also compatible to 4xUB953 ?

Best regards,
Andy
Hello Andy,
Yes, the UB962 is compatible with UB953. You need only to make sure you do not have more than 2.528 Gbps CSI-2 Video Bandwidth Per Channel.
Oh Sorry, I was thinking of the UB960. Ofcourse the 960 has only 1x CSI-2 port, so it can't handle these datarates.
The 962 can support max output bandwidth = 5.6Gbps, means 1.4Gbps CSI data per each RX port.
Andy,
the 962 can support 4x2Mp Cameras but not in 4*16 format.
to be able to support the 4*16 format you need a much higher CSI bandwidth. We may discuss this via email since this is a public forum.