Part Number: TUSB212
Dear Pals,
I have chose TUSB212 to improve USB signal quality on FR-4 PCB board,I'm confused with the location of TUSB212,near USB PHY or near USB connector or midway?Pls help to solve the question,Thanks!
More information:1.The USB signal from USB PHY to Connector is far more than 16 inchs which is the maxmum length requirement of USB PHY when not use USB hub or redriver;
2.According to SLLA392,TUSB212 can pass at least 0.5m AWG28 at condition"Max Post-Channel Loss to Pass (near end eye mask)";It seems that the TUSB212 can be palced nearby USB connector;


Best Regards,
Ji;