This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

XIO2001: Surface temperature Tc

Part Number: XIO2001


Hello,

Please tell me the following four points in the XIO2001 PNP PowerPAD HTQFP Package. 

I want to know the maximum and minimum values of the surface temperature Tc.

I think it can be calculated as follows, but is it correct? [Tc_max = Tj_max - θjc x Pmax = 105 - 18.9 x 0.954 = 87.0]

②What are the conditions that is power consumption and the solder bonding ratio of the Power PAD for the value of ①?

③Does the maximum and minimum value of Tc change depending on the solder bonding ratio of the Power PAD? 

④When ③ is YES, please use a graph to tell us what kind of transition. 

Best Regards,

T. Fukuoka