This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS90UB941AS-Q1: please help provide one sample configuration for splitter mode.

Part Number: DS90UB941AS-Q1

Hi TI:

      Please help provide one sample configuration for splitter mode. Thanks.

        941->>928/926

       link0:

    800*480: hwh:16, hbp:48, hfp:32, vwh:2, vbp:2 vfp:4 

       link1:

   720*720: hwh:4, hbp:40, hfp:44, vwh:4, vbp:22, vfp:16

  • Hello Chen,

    Can you please share the panel specifications for both panels here? Keep in mind that 941AS does not have control over creating specific vertical blanking components for each split screen. The blanking for each side is based on the vertical timing of the superframe which contains both images, and then the smaller screen will also see additional vertical blanking equal to the cropped out lines which in this case would be 720-480 = 240 extra vertical blanking lines which may or may not be compatible with your panel. We can verify with the panel specifications which show the tolerance of the timing parameters 

    Best Regards,

    Casey