This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Please recommend a switch device for Packet Transport Network

Guru 12825 points

Other Parts Discussed in Thread: DS100MB203, DS250DF230, DS125DF1610, DS250DF410, DS280DF810

Hello,

My customer is looking for an on-switch device for PTN(Packet Transport Network) application.

    1. Unit

           - Line side : SFI(SFP+) 4 Port

           - System side(Host side) : 10GBase-KR 4 Lane x 2 Slot

    2. Device requirements

           - Built-in 1:2/2:1 MUX or 2x2 Cross-Point Switch (For host-side switching)

           - Host side SerDes Auto-Training

           - Including SerDes tunning parameter (Amplitude, Equalizer, Pre/De-emphasis)

           - Recovery clock(Option)

Please recommend the most suitable product to implement the above function.

Thank you.

JH

  • Pls take a look DS100MB203 or DS250DF230 .

  • Hi Brian,

    Thank you for your help.

    My customer has some questions about DS100MB203 device.

         1. The DS100MB203 has 'Host side SerDes Auto-Training' function ?

         2. In the case of D_INx and S_OUTx paths, is the SPDT switch built-in? Is it possible to operate with a common connection as well?

    In addition, are there any products with built-in mux among Retimer products?

    Thank you.

    JH

  • Hi,

    1. The DS100MB203 does not implement auto-training, However, it implements a highly linear data path which allows for the host ASIC auto-negotiation and link training data to be passed through it transparently
    2. I believe this is possible. It would be good though if you can provide block diagram to illustrate what the customer can do, just so that there is no misunderstanding

    Within the TI retimer portfolio, the DS125DF1610 10G/12.5G retimer has 4x4 crosspoint mux. All of the 25G retimers have 2x2 crosspoint: DS250DF410, DS280DF810, DS250DF230