Part Number: DS90UH928Q-Q1
Hi team,
There is a description about OEN toggling limitation below.
1. Is this a mandatory requirement?
2. Could you explain step by step why horizontal pixel shift at the LVDS occur?
3. If 0x01[0] digital reset is set, LOCK will be lost? If yes, it will take another 40ms(max) to relock?
9.4 OEN Toggling Limitation
EON should be enabled LVDS outputs after PDB turns to high state and the internal circuit is stabled. Since OEN
function is asynchronous signal to the internal digital blocks, repeated by OEN toggling may result in horizontal
pixel shift at the LVDS output. TO avoid this, recommend to reset by programming Register 0x01[0] for digital
blocks after OEN turn to ON state.
regards,