Part Number: TUSB321AI
Hi All,
can you please tell if the TUSB321AI is in configure as UFP, and it will try to communicate out the power level that it can consume.
When it detects then he will tell the system through OUT1 and OUT2 the power that it can use.
My question is will the TUSB321AI in UFP first ask for 5V 3A, and then 5V 1.5A, and then 5V (0.9A for USB3 , 0.5A for USB2) ? in that order?
Best Regards,
David.