This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS65987D: GUI 6.1.2 Changelog

Part Number: TPS65987D

Hello,

Is there a changelog for version 6.1.2 of the GUI tool?

Possibly related, my customer is seeing an issue where they cannot set two GPIOs to the same event in version 6.1.2. Specifically, they would like to have GPIO 0 and GPIO 19set to “Port 0 DP Mode Select Event” (event 41). In version 6.1.1, they were able to accomplish this without any issue. In version 6.1.2, they can set one GPIO appropriately, and when they set the other GPIO, the first GPIO will be set to event -2, “Disabled”. Is this expected behavior?

Thanks,

Michael

  • ,

    Yes, see the email I sent for the internal changelog for the tool.

    Yes, this is the expected behavior. 6.1.1 included a bug where two different GPIOs could be set to the same GPIO event. This is not supported by the device, so 6.1.2 properly changes any duplicated event to Disabled, giving priority to the GPIO the user last interacted with.