Part Number: TCAN1051H
Other Parts Discussed in Thread: TCAN1042HG, TCAN1042H
We are looking for an alternate to TCAN1051HDR that is both 70V bus tolerant and an SOIC packaging. (H) and (HG) are two transceivers that we’ve already been searching the market to buy and use in our design. (HV) and (HGV) are two other alternates I’ve been considering that include a level shifter on pin 5. I am wondering if the level shifter on pin 5 needs to be connected in order for the transceiver to work or if it can be left floating? Pin 5 in our design is left floating, so I am wondering if we can actually use (HV) and (HGV) as alternates for (H) and (HG)?