Part Number: SN75DP126
Other Parts Discussed in Thread: TS3DV642, TDP158, HD3SS214
Hi Team,
The customer is asking that do we have the similar function device as below which can support up to DP 1.4? I think SN75DP126 should be okay, but it only support DP1.2.
Or they have to add a TS3DV642 as DP++ input and TDP158 on the HDMI port? Thank you.

Best regards,
Mike