Part Number: TUSB2036
I am using TUSB2036 in my circuit , and made the MODE low to select 6MHz . But while checking using oscilloscope i am not getting anything. I have attached my circuit.
Kindly provide any solution for the same.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TUSB2036
I am using TUSB2036 in my circuit , and made the MODE low to select 6MHz . But while checking using oscilloscope i am not getting anything. I have attached my circuit.
Kindly provide any solution for the same.
Hi Dinesh,
The capacitor needs to be attached to the RESET pin directly, not the 3.3V rail.
Are any downstream devices connected to the hub? The host may put the hub in a low power mode (crystal turns off) if no downstream devices are connected.
Regards,
JMMN
sir,
As you told ,I connected capacitor directly to reset pin respected to ground without connecting it to power rail (3.3V).while powering on , i got the frequency for some 2 seconds and it stopped after that. It was 50mA when the crystal showed signal ,then when it reduced to 40mA i only got voltage around 1.5V at XTAL1 pin and in 30mA no response was there in tat pin.
I repeated three time after that .I got only 1.5V ( 40mA ) and no response that's crystal off (30mA).
Hello Dinesh,
You mentioned that the yellow mark shows the reset pin connection, but in that case RESET is connected to a pullup and the capacitor is connected to the 3.3V rail, not the RESET pin. If the capacitor is connected directly to the pin, the reset timing is ok.
Are there any downstream devices connected? It sounds like the hub is entering suspend mode since no devices are connected.
Regards,
JMMN
Hi,
Yeah ,i had done the said modification by you in the hardware part and checked the clock frequency for 6MHz,
faced the same issue(above mentioned amps details) as i mentioned before. I have connected three downstream devices with the IC.
Three connection form TUSB2036 connected to three MCP2200 IC ( USB to UART converter ) and then to the device.MCP2200 also has crystal (12MHz) working perfectly.
Can you check the line states on DP0 and DM0. DP0 should be pulled high when the hub is attached to the host and then there should be some signaling from the host, does that occur? What operating system is running on the host?
Regards,
JMMN
Its partially working now and i getting 6MHz in pin29(XTAL2).Now the issue is i am not getting 6MHz constantly in pin30(XTAL1).While placing a DSO probe in XTAL1,i am getting 6MHz for 2 second and it reduces suddenly. Again if i place probe i get it and will go after 2 second ,then taking the probe out and place again will get 6MHz for 2 second, its not constant as i m getting in pin29(XTAL2)
Ok, the load capacitance looks correct. Can you confirm that both caps are grounded, I see a ground symbol on both caps but only one has a DGND signal connection? Are you seeing the same issue across multiple boards?

Now have taken new board and populated all components same as i did in the previous board . Now i facing same issue in the crystal past. Power everything in check ,everything is ok ,but only the crystal portion i m not getting anything.