Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ESD321: alternatives

Part Number: ESD321
Other Parts Discussed in Thread: TPD1E04U04, STRIKE

Hello,

We are having trouble sourcing the ESD321DPYR. Are there any pin to pin or similar alternatives that have more stock for us to pivot to?

Thanks,
Adam

  • Hello Adam,

    Two good alternatives to ESD321DPYR would be either ESD351DPYR and TPD1E04U04DPYR. Both are single channel 3.6 V unidirectional diodes and P2P compatible. According to ti.com, it looks like TPD1E04U04 is the only part currently in stock, and it is only available in a tape instead of a reel (TPD1E04U04DPYT).

    Another option could be to use a bidirectional diode instead of a unidirectional one. The main drawback would be that it would offer less protection in the event of a negative ESD strike compared to a unidirectional diode. TPD1E1B04DPYT would be a good replacement if you were to choose this option, and it has much more stock than TPD1E04U04DPYT. 

    Would either of these options be sufficient?

    Regards,

    Matt Smith