Part Number: DS90UH940-Q1
Hi Team,
Can you help with the question below from Panasonic?
"Below are the register settings we have done for Audio on ds90uh940:
|
22h |
Datapath_Control |
R/W |
0x00 |
Correct settings are sent from the mating serializer |
|
28h |
Datapath_Control_2 |
R/W |
0x00 |
Correct settings are sent from the mating serializer |
|
2Bh |
I2S_Control |
R/W |
0x01 |
Bit 3 set when I2S FIFO Overrun, Bit 2 set when I2S FIFO Underrun, Bit 1 clears FIFO Error, Bit 0 is I2S Edge Select |
Can you please check this register settings and let us know if any other settings are required?"
It looks like some settings are auto-loaded by the serializer (I believe they plan to use UH949), but it isn't entirely clear to me if there are other register settings that must be changed to support audio.
Thanks,
Ben