Part Number: TUSB2077A
Hello Team
We are using TUSB2077A with custom board & problem we are facing is no downstream ports are getting enumerated with this USB Hub. When measured we found that pin no.1 i.e Suspend pin remains high i.e between 2.7V to 3.3V whenever external host is plugged in on Upstream port I have attached snap of my Schematic design All downstream ports have a pull-up on OVERCURRENT pin & setting as mentioned in my Schematic.
1) What are the sequence required to be followed detect the downstream port on TUSB2077A and getting it enumerated ?
2) Is there any specific drivers/commands required to be installed/followed on Linux/Windows PC for the same?
3) Do you suspect any issue in the hardware design here? We already followed all the guideline provided.
Appreciate your help in Advance.