Part Number: DP83620-EVK
Other Parts Discussed in Thread: DP83620, TIDA-00928
Hello,
I'm working on DP83620-EVK with a 1000BASE-SX SFP Transceiver. But no traffic is observed.
The phy is configured in fiber mode (i.e: FX_EN):
- If I set the loopback (MII) the packets are sent and received correctly (so the phy configuration seems correct).
- If I create a loopback with the fiber, nothing is received.
I'm not sure about the compatibility between the phy and the transceiver.
Can a 100BASE-FX phy work with a 1000BASE-SX Transceiver or do the phy and tranceiver base have to match ?
Registers values:
[0x00] 0x2100
[0x01] 0x78c9
[0x02] 0x2000
[0x03] 0x101
[0x04] 0x0
[0x05] 0x4
[0x06] 0x3
[0x07] 0x0
[0x08] 0x14b
[0x09] 0x1
[0x0A] 0x21
[0x0B] 0x2
[0x0C] 0x0
[0x0D] 0x0
[0x0E] 0x0
[0x0F] 0x0
[0x10] 0x0
[0x11] 0x0
[0x12] 0x0
[0x13] 0x0
[0x14] 0x0
[0x15] 0x0
[0x16] 0x0
[0x17] 0x0
[0x18] 0x0
[0x19] 0x0
[0x1A] 0x0
[0x1B] 0x0
[0x1C] 0x0
[0x1D] 0x0
[0x1E] 0x0
[0x1F] 0x0
Best regards
Thibaut