This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TUSB8044A: New project USB3.1 Hub chip requirements

Part Number: TUSB8044A
Other Parts Discussed in Thread: TUSB8043A, TUSB8042A

Hi TI team,

Is there any recommended universal USB3.1 Hub chip model and corresponding evaluation kit that meets the following selection requirements and has been mass-produced? Currently TUSB8044A is initially selected. Please help to confirm whether the universal part number is available?

The selection requirements are as follows:

1.USB3.2 x1 Gen1(5 Gbps)hub

2.USB3.1 Hub 14

3.upstream支持SS/HS USBdownstream支持SS/HS/FS/LS USB

4.工业级。

5.成本较低。